SRM motor control with hall sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRM motor control with hall sensor

1,672 Views
Kaarthi
Contributor II

Hi,

I am using MKV30F128 micro controller for controlling 3 phase SRM motor with hall sensor feedback for position measurement. I am able to rotate the motor in no load. In load the over current fault occurs even with low load. In no load also, the 3 phase currents are not equal. Anyone having experience with SRM motor control, kindly help me to solve this problem.

Note: feedback - magnet disc is attached with shaft and hall sensor is placed against it.

0 Kudos
Reply
1 Reply

1,661 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, kaarthi,

I think it is reasonable that phase current is high when you connect the load. Can you adjust the peak current threshold so that the current fault does not happen.

Pls go to the link and download DRM100.pdf for the phase current waveform

https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/RDDSCSHSSR-Sensorless-High-Speed-SR-Motor-Dr...

 

BR

XiangJun Rong

0 Kudos
Reply