SRAM size and location for MK64FX512VLL12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SRAM size and location for MK64FX512VLL12

跳至解决方案
2,241 次查看
steve32768
Contributor II

Can someone from NXP please confirm the SRAM size and address range for the MK64FX512VLL12?

Per the datasheet, this should be 256KB, but there's conflicting information in the reference manual. The reference manual indicates a size of 256 KB, but address range of 0x1FFF_0000-0x2001_FFFF (which is only 192 KB)

See attached picture from the table in section 3.5.3.1 of the latest reference manual v.5. 

标签 (1)
0 项奖励
回复
1 解答
2,224 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Interal concurred with the documentation error. The address ranges of all the listed devices should be 0x1FFF_0000 - 0x2002_FFFF. Thanks for reporting this mistake.

在原帖中查看解决方案

3 回复数
2,220 次查看
steve32768
Contributor II

Thanks for the quick reply on that!

0 项奖励
回复
2,231 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, the MK64FX512VLL12 has 256 KB of SRAM. Still, I will escalate your remarks on the address ranges in the Reference Manual as a possible documentation error and will get back to you as soon as I receive a response.

 

Regards,

Edwin.

2,225 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Interal concurred with the documentation error. The address ranges of all the listed devices should be 0x1FFF_0000 - 0x2002_FFFF. Thanks for reporting this mistake.