SPI1 dma source - FRDM-K22F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI1 dma source - FRDM-K22F

Jump to solution
2,020 Views
errorek123
Contributor III

Hello,

I'm writing some code to handle SPI dma transfer but it seems like K22 chip got common source for TX and RX for SPI1. Does it mean it can be either be used for receive data or transmit data and it can't be used for both? Is there any workaround or i have to live with that or switch SPI0 if both rx and tx dma is needed?

Tags (3)
0 Kudos
Reply
1 Solution
1,823 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Brian Smith ,

  Your are right, in the FRDM-K22 on board K22 chip, the SPI1 share the transmit and receive request.

  So, in my opinion, if you want to use both the Transmit and receive DMA function, it's better to use SPI0 interface, it has the separated request source:

pastedImage_1.png

Wish it helps you!

If you still have question about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,824 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Brian Smith ,

  Your are right, in the FRDM-K22 on board K22 chip, the SPI1 share the transmit and receive request.

  So, in my opinion, if you want to use both the Transmit and receive DMA function, it's better to use SPI0 interface, it has the separated request source:

pastedImage_1.png

Wish it helps you!

If you still have question about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply