SPI of MKE04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI of MKE04

897 Views
thomaswu
Contributor I

I am used the MKE04Z128, and the SPI which set the clock is about 10M, but the time of two datas which are sent is so long,  is there any peple has this problem? and how can I solve this problem, and I am use the PE, and which help me do the initial of spi and so , ..

0 Kudos
Reply
1 Reply

813 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Would you please attached the project and waveform of SPI?

Have you try to test the SPI example in SDK_2.4.0_MKE04Z128xxx4, will it show the same phenomenon?

SDK_2.4.0_MKE04Z128xxx4 spi.png

1 Build SDK.png

2 Download SDK.png3 Download SDK Archive.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply