SPI maximum frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI maximum frequency

2,214件の閲覧回数
aescov
Contributor I

Regarding K26P169M180SF5 SPI bus speed:

 

From the datasheet the maximum SPI frequency (Master mode) is specified for two voltage ranges:

 

2.7V < Vcc < 3.6V: 30MHz

1.71V< Vcc < 3.6V: 15MHz

 

For our application, running at 1.8V, this becomes a problem!

 

What is the limiting factor for the maximum SPI frequency and would it be possible to run the SPI at 30MHz even when Vcc=1.8V?

0 件の賞賛
返信
1 返信

1,851件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

As datasheet shows: The DSPI module can operate across the entire operating voltage for the processor, but to run across the full voltage range the maximum frequency of operation is reduced.
When the VCC =1.8V, the Max. SPI baud rate is 15Mbps.

When the VCC = 1.8V,  the SPI communication signal quality could be interfered by external EMI and generate SPI communication problem with higher baud rate.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信