SPI communication on KL25Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI communication on KL25Z

2,776件の閲覧回数
michelmeunier
Contributor I

Hello,

I tried to read an ADXL345 accelerometer, I have written my own SPI read and write because it doesn't work with processor expert.

The initialization of SPI is:

--------------------------------------------------

  SIM_SCGC5 |= SIM_SCGC5_PORTD_MASK;  //Turn on clock to D module
  SIM_SCGC4 |= SIM_SCGC4_SPI0_MASK;   //Enable SPI0 clock

  PORTD_PCR0 = PORT_PCR_MUX(0x2);//Set PTD0 to mux 2 [SPI0_PCS0]
  PORTD_PCR1 = PORT_PCR_MUX(0x2);//Set PTD1 to mux 2 [SPI0_SCK]
  PORTD_PCR2 = PORT_PCR_MUX(0x2);//Set PTD2 to mux 2 [SPI0_MOSI]
  PORTD_PCR3 = PORT_PCR_MUX(0x2);//Set PTD3 to mux 2 [SPIO_MISO]

  SPI0_C1 = SPI_C1_MSTR_MASK | SPI_C1_SSOE_MASK | SPI_C1_CPHA_MASK | SPI_C1_CPOL_MASK;   //Set SPI0 to Master & SS pin to auto SS

  SPI0_C2 = SPI_C2_MODFEN_MASK;   //Master SS pin acts as slave select output

  SPI0_BR = (SPI_BR_SPPR(0x02) | SPI_BR_SPR(0x08)); //Set baud rate prescale divisor to 3 & set baud rate divisor to 64 for baud rate of 15625 hz
  SPI0_C1 |= SPI_C1_SPE_MASK;//Enable SPI0

  WAIT1_Waitms(500);

------------------------------------------------------------

the read function is quite simple, I write the adress and next read the answer;

-------------------------------------------------------------

uint8_t retour=0,dummy;

bool fini=FALSE;

  while(!(SPI_S_SPTEF_MASK & SPI0_S))

      {

      //While buffer is not empty do nothing

      }

    SPI0_D =adresse+0x80;//write adress+0x80 (read mode)

    while(!(SPI_S_SPRF_MASK & SPI0_S))

    {

      //While received buffer is not full do nothing

    }

    retour=SPI0_D;

    return retour;

-------------------------------------------------------

For the test I init the SPI and try to read adress 0x00.

As you can see on the analyzer image, the byte is written, but nothing is read, the KL25Z do nothing. I should have a second set of 8 clock pulses.

analyser.jpg

Michel

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

2,485件の閲覧回数
mjbcswitzerland
Specialist V

Hi

In order to send an address and then read a further byte you must send two bytes:

- the address

- a 'dummy' one (eg. 0xff) - this will generate the second 8 clocks

- they you will receive the result value back

Regards

Mark

0 件の賞賛
返信

2,485件の閲覧回数
michelmeunier
Contributor I

Thank you Mark, you have solved a part of my problem.

Now the picture of analyzer seems to be correct, but the SPRF bit seems to be unused. I have add a 5ms wait before to read the answer, I should received 0xe5 but I allways get 0!!.

My read function looks like that:

------------------------------

uint8_t retour=0,dummy;

    bool fini=FALSE;

    while(!(SPI_S_SPTEF_MASK & SPI0_S))

      {

      //While buffer is not empty do nothing

      }

    SPI0_D =adresse+0x80;//write adress+0x80 (read mode)

    while(!(SPI_S_SPTEF_MASK & SPI0_S))

      {

      //While buffer is not empty do nothing

      }

    SPI0_D =0x00;//write 0x0 to generate 8 clock pulses

    while(!(SPI_S_SPRF_MASK & SPI0_S))

    {

      //While received buffer is not full do nothing

    }

    WAIT1_Waitms(5);

    retour=SPI0_D;

    return retour;

----------------------

And the analyzer:

analyser.jpg

I think I am that with your help, I am very closed from the solution.

Thanks

Michel

0 件の賞賛
返信

2,485件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Michel Meunier,

   Actually, to KL25Z, you don't need to delay after the SPRF is set, you can read the D register directly, and try again.

  If you still not OK, please add the dummy read:

uint8_t retour=0,dummy;

    bool fini=FALSE;

    while(!(SPI_S_SPTEF_MASK & SPI0_S))

      {

      //While buffer is not empty do nothing

      }

    SPI0_D =adresse+0x80;//write adress+0x80 (read mode)

    while(!(SPI_S_SPTEF_MASK & SPI0_S))

      {

      //While buffer is not empty do nothing

      }

    dummy = SPI0_S;

    SPI0_D =0x00;//write 0x0 to generate 8 clock pulses

    while(!(SPI_S_SPRF_MASK & SPI0_S))

    {

      //While received buffer is not full do nothing

    }

    retour=SPI0_D;

    return retour;

Wish it helps you!

If you still have question, please let me know!

Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,485件の閲覧回数
mjbcswitzerland
Specialist V

Michel

After you configure the SPI interface add

(void)SPI0_S;

(void)SPI0_D;

This will ensure that the status flags start to work correctly.

Regards

Mark

0 件の賞賛
返信