SPI always reads zero???

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI always reads zero???

9,091件の閲覧回数
jonathanscott
Contributor III

Well, this is somewhat embarrassing, but I'm finally frustrated enough to ask for help.  I have a simple routine to read 3 bytes from the SPI.  It worked just fine through months of development, and then something changed, and now it always returns zeros despite the correct data clearly present on a scope (screenshots attached).  This is an MK10DX128VMP5, using the IAR tools, with the SPI routines and drivers generated by PE.  What I should get is statbyte[0] = 0x40, statbyte[1] = 0x00, and statbyte[2] = 0x0B, but instead they are all 0x00.

MYSPI_ClearRxBuf();

STROBE_MISO_PutVal(1);                               //strobe is done with GPIO pins

STROBE_MISO_PutVal(0);      

for(i=0; i<3; i++){ 

  MYSPI_SendChar(0x00);                                 //clock in a char

spibyte = MYSPI_RecvChar(&statbyte[i]);   //get it

}

STROBE_MISO_PutVal(0);

Does anybody know what's going on?  I also attached a screenshot showing the spi configuration registers.

Thank you!!!

ラベル(1)
タグ(2)
3 返答(返信)

8,596件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Have you maybe overwritten the SPI-RX input pin configuration so that it doesn't see the data?

Regards

Mark

8,598件の閲覧回数
jonathanscott
Contributor III

Good thought, Mark, but the pin configuration appears to be correct.  I made some other changes, and now it's magically working again.  I'll repost if it happens again.

Thanks,

Jonathan

8,598件の閲覧回数
M_Grillo
Contributor III

Hello,

I'm having the same issue. What did you change to get MISO to work and not always report 0's?  I'm using a K60D100 TWR board and trying to get SPI2 to work on PORTB(pins 20-23). Tried every example but no luck. MOSI, ,CLK and CS work fine.

Pin setup:

As a sanity check a tried grounding SIN (0x00..) and then tried tying SIN to 3.3V (0xffff...) Still read all 0's.

/* Configure PINs  */

                PORTB_PCR20 = (0|PORT_PCR_MUX(2));        //0x200; // Alt2 //CS

                PORTB_PCR21 = (0|PORT_PCR_MUX(2));        //0x200; // Alt2 //CLK

                PORTB_PCR22 = (0|PORT_PCR_MUX(2));        //0x200; // Alt2 //SOUT

                PORTB_PCR23 = (0|PORT_PCR_MUX(2));        //0x200; // Alt2 //SIN

Using MQX 4.1.1 w/DMA on SPI2

Thanks,

Mark