SPI Documentation Error - protocol clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPI Documentation Error - protocol clock

跳至解决方案
3,534 次查看
pmcl
Contributor I

Hi All,

I'm looking at the K70 Reference Manual, Chapter 54, SPI.

In the section on the SPIx-CTARn, pages 1815 onwards, it mentions 1/fp in various formula.

I'm trying to set up a "Delay After Transfer". According to page 1818:

"The Delay after Transfer is a multiple of the protocol clock period, and it is computed according to the following equation:

t(DT) = 1/fp x PDT x DT"

This means that 1/fp is the protocol period, and fp is meant to stand for the protocol frequency (bit rate).

However, upon testing, it appears that the delay seems to be a multiple of the module clock, not the protocol clock. I'm using a protocol clock of 1 MHz and a module clock of 25 MHz, and the delay is exactly 25 times smaller than the formula.

Is the documentation wrong? Should it say "module clock" rather than "protocol clock" and therefore all the other formulas/wording needs to change too? Is this a common problem across the Kinetis family?

0 项奖励
回复
1 解答
3,400 次查看
melissa_hunter
NXP Employee
NXP Employee

Hi Peter,

Yes, thank you for reporting the issue. I entered in a PDM ticket against the manual requesting to have this fixed. The manual did get an update somewhat recently, so I doubt the documentation team will get to this any time soon.

If you need the updated documentation, let me know and I'll see what I can do to expedite.

Regards,

Melissa

在原帖中查看解决方案

5 回复数
3,400 次查看
cutworth
NXP Employee
NXP Employee

Hi Peter,

Yes, this is not that clear when using fp to represent module clock. This has been fixed with other Kinetis document where it is changed to fsys. 

Hao

0 项奖励
回复
3,400 次查看
pmcl
Contributor I

Hi Hao,

Thanks for the quick response.

It's not just the "fp" that's the problem - the descriptions explicitly mention "protocol clock", not "module clock", so the wording that goes with fp needs to change.

Anyway, I was looking for a way to point out the error to someone in NXP - didn't see a direct link to "report an error", so I posted on the forum.

Thanks for your help.

PMcL

0 项奖励
回复
3,400 次查看
cutworth
NXP Employee
NXP Employee

Hi Peter,

Thanks for reporting the documentation error. I will let associated person know this.

melissah‌ Could you help look at this reported documentation issue for K70 SPI module?

Hao

0 项奖励
回复
3,401 次查看
melissa_hunter
NXP Employee
NXP Employee

Hi Peter,

Yes, thank you for reporting the issue. I entered in a PDM ticket against the manual requesting to have this fixed. The manual did get an update somewhat recently, so I doubt the documentation team will get to this any time soon.

If you need the updated documentation, let me know and I'll see what I can do to expedite.

Regards,

Melissa

3,400 次查看
pmcl
Contributor I

Hi Melissa,

I'm fine with the current documentation - now that I know about the error.

Thanks for your assistance.

Regards,

PMcL

0 项奖励
回复