SPI Bus KL02Z32M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Bus KL02Z32M

2,023 Views
danielromuald
Contributor I

it is possible to receive a 24 bits word through the SPI bus of the KL02Z32M microcontroller. if yes how? 

0 Kudos
Reply
2 Replies

1,873 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Danel

No, you cannot receive 24bits once. You need to receive 8-bits four time, then combine to a 24-bits word.

Hope it can help you.

Best Regards

Paul

0 Kudos
Reply

1,873 Views
danielromuald
Contributor I

Thanks paul,

The problem is that i have 24 pulse clock (SCK) in just one chip select

(PCS) for all. So my microcontroller read just the 8 first MSB of my 24

bits.

Best regards,

Daniel

Le 24/09/2015 11:28, Paul.Tian a écrit :

>

Freescale Community

<http://jiveon.jivesoftware.com/mpss/c/mAA/PDcDAA/t.1qp/IbaUxWT_TIqxw2QjUcBPwA/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

<http://jiveon.jivesoftware.com/mpss/c/mAA/PDcDAA/t.1qp/IbaUxWT_TIqxw2QjUcBPwA/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

>

SPI Bus KL02Z32M

reply from Zhe Tian

<http://jiveon.jivesoftware.com/mpss/c/mAA/PDcDAA/t.1qp/IbaUxWT_TIqxw2QjUcBPwA/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSOlIuxtIkSGV6JrWax7EVCFhg9sux7Y-2BWTD2lI7iNTB3V6kmNHTq0J6ckeuINCvu0-3D>

in /Kinetis Microcontrollers/ - View the full discussion

<http://jiveon.jivesoftware.com/mpss/c/mAA/PDcDAA/t.1qp/IbaUxWT_TIqxw2QjUcBPwA/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSMM4An076D-2BOgAh4rZRV-2FHM58yi50BtgQgM4SvEhnsyRTuFvrvhvo1CiTMnLUDIqs-3D>

>

0 Kudos
Reply