SH1106 Drive Library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SH1106 Drive Library

3,680 Views
assisantunes
Contributor I

Hi all,

I am developing a project with MKE02Z64 and a graphic display SH1106 in KDS. Which library can I use for the SH1106 drive?

0 Kudos
Reply
3 Replies

3,404 Views
assisantunes
Contributor I

Hi,

The datasheet is attached. I use the 128x64 model with I2C communication.

0 Kudos
Reply

3,404 Views
BlackNight
NXP Employee
NXP Employee

There is a Processor Expert component (SSD1306) for the SH1106 (which is a variant of the SSD1306):

pastedImage_2.pngpastedImage_1.png

The component is availble on SourceForge (latest release: McuOnEclipse Components: 1-Apr-2018 Release | MCU on Eclipse ). If you want to use the library without Processor Expert: see GitHub - ErichStyger/McuOnEclipseLibrary: Library of McuOnEclipse components .

An example project is availble here: mcuoneclipse/Examples/KDS/FRDM-K64F120M/FRDM-K64F_SSD1306 at master · ErichStyger/mcuoneclipse · Git... 

I hope this helps,

Erich

0 Kudos
Reply

3,404 Views
miduo
NXP Employee
NXP Employee

Hi,

Sorry, I am not familiar with the SH1106 display you mentioned. Would you mind to share the datasheet or fact sheet for this part?

0 Kudos
Reply