SH Card Code for K-20

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SH Card Code for K-20

1,519件の閲覧回数
moiz_husain
Contributor I

Hi I am Interfacing SD card with SPI in Kineties K-20.

how to write code for it any one can help with example for k-20

ラベル(1)
0 件の賞賛
返信
1 返信

1,443件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Moiz,

I'd like to suggest that you'd better to choose the SDHC module for operating SD card instead of SPI interface.

FSL hasn't provided the similar demo to meet your requirement, however I'd like to share a post with you and I think it shows the way to make it.

please check the link as below.

Arduino Data-Logger Shield with the FRDM-KL25Z Board | MCU on Eclipse

Hope it helps.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信