SDK that support KSZ8041NL for K64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK that support KSZ8041NL for K64

1,794 Views
fshah30
Contributor II

Hi,

Please let me know how I can utilize the SDK from FRDM-K64 board. I am using KSZ8041 PHY on the prototype and want to convert the driver of KSZ8081 which is available in SDK for FRDM-K64. I try to use the same driver but it shows Initialization is fail!!....

 

0 Kudos
Reply
2 Replies

1,772 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @fshah30,

As you mention, we only provide SDK support for the KSZ8081. Since it is a third party phy, I’m not able to point out any differences that stand out between this and the KSZ8041, so the only viable solution would be to look into both datasheets for these differences and modifying the code accordingly.

Sorry for the inconvenience this may cause.

 

BR,

Edwin.

0 Kudos
Reply

1,765 Views
fshah30
Contributor II

Thank you

0 Kudos
Reply