SDK error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK error

2,095 Views
bendelathouwer
Contributor I

after importing an SDK(version 2.7.0 for the kintis K64) in the mcuxpresso ide i get the error unable to find the manifest fil in the sdk zip and that the file is invalid And i got the sdk from the SDK builder site. 

Does anyone know what I did wrong?

Thank you in advance and with best regards Ben  

Labels (1)
0 Kudos
Reply
3 Replies

1,980 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Ben:

Which IDE you are using?

SDK 2.7 should work with MCUXpresso IDE 11, please download the latest IDE from

MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE) | NXP 

Regards

Daniel

1,980 Views
bendelathouwer
Contributor I

Thank you verry mutch !

I was using the old ide and that must be the reason it didn't work. Also a second question.Is there an easy way of toggling a pin  I asume using the GPIO_Porttoggle command but how do i use it ? 

thank you in advance and with best regards Ben 

0 Kudos
Reply

1,980 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Ben:

There is one GPIO example project demonstrates how to toggle a GPIO pin

Please refer to demo drivers/gpio/led_output

The example is supported by the set, clear, and toggle write-only registers for each port output data register. The
example take turns to shine the LED.

Regards

Daniel

0 Kudos
Reply