SDK build: No middleware selection for Channel sounding

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK build: No middleware selection for Channel sounding

2,474 Views
BLEDev
Contributor II

Hello,

I'm trying to build SDK and run channel sounding examples on KW45 LOC board following this user manual KW45B41Z-LOC Board User Manual (nxp.com).

BLEDev_1-1720497611759.png

 

But it seems SDK builder has no option Middleware "Wireless Localization". Could you help check?

BLEDev_2-1720497666201.png

 

Thanks

 

0 Kudos
Reply
7 Replies

558 Views
BLECSEval
Contributor I

Hi Ricardo,

I am seeing the same issue when doing channel sounding evaluation with KW45B41Z-LOC boards. There is no "Wireless Localization" Middleware when building/downloading the SDK.

Can you please send me the SDK with wireless localization middleware and the wireless_ranging example/project? Really appreciate if you can send me "AN13974 - Bluetooth Low Energy Localization Application Note" as well.

Thank you!

 

0 Kudos
Reply

2,290 Views
sysumst111
Contributor I

Hey, have you received the 'Wireless Localization' SDK? I'm also trying to run the channel sounding examples. If you have it, could you please send me a copy as an attachment? Much appreciated

0 Kudos
Reply

2,448 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Do you have the KW45B41Z-LOC?

 

I sent you a private message.

 

Best Regards,

Ricardo

0 Kudos
Reply

248 Views
Fabian555
Contributor I
I am exploring Channel Sounding using the KW45B41Z-EVK. Are these wireless localization examples still available? If so could they be shared? I am also not finding any info about them in SDK builder.

Best Regards,
Fabian
0 Kudos
Reply

1,850 Views
aliyasser7
Contributor I

Can you send me the wireless localization SDK also?
I have been reviewing the AN13974 - Bluetooth Low Energy Localization Application Note (Rev. 1.2, June 2024) and would like to implement the solutions described in the document. However, I am unable to locate the associated code or SDK examples referenced within the application note.

0 Kudos
Reply

2,226 Views
jorisvergeer2
Contributor I

@Ricardo_Zamora Can you send me the wireless localization SDK also?

I have KW32W148, but that should also KW45 code. I'd be completely happy if Channel Sounding and Ieee802.15.4 can run both on the same board. I need the results of Channel Sounding to be transmitted over Ieee802.15.4 to our data collection network. 

0 Kudos
Reply

2,318 Views
sysumst111
Contributor I
I have the same problem, can you send me a private message?
0 Kudos
Reply