SDK about the chip MK20DX256VMD10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK about the chip MK20DX256VMD10

1,991件の閲覧回数
ww_dong
Contributor I

HI:

    I use a chip (MK20DX256VMD10) on the board, I download the sdk by the processor,the software include a TWR-K60D100M KIT sample automatically. Now i want to use the MCUXPRESSO CONFIG TOOL to transform the SDK and sample to  Keil project,but the MCUXPRESSO CONFIG give a error:

the mean is:the device detected from the project is not the same to the given device (MK20DX256xxx10), so the generated keil project ,i can open and build with no any error,but all the information about the device is KN60DX10.

   I could not find a exactly sdk and develop board  according to MK20DX256VMD10(MK20DXXX),What can i do ?

          Thanks

0 件の賞賛
返信
1 返信

1,980件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @ww_dong ,

Yes, if you create a new project base on MK20DX256 SDK, the project is only for TWR-K60M100. All the SDKs are around TWR/FRDM board.

You can replace those K60 files with K20 files manually.  But that's a bit boring. 

 

Regards,

Jing

0 件の賞賛
返信