SDK about the chip MK20DX256VMD10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK about the chip MK20DX256VMD10

1,474 次查看
ww_dong
Contributor I

HI:

    I use a chip (MK20DX256VMD10) on the board, I download the sdk by the processor,the software include a TWR-K60D100M KIT sample automatically. Now i want to use the MCUXPRESSO CONFIG TOOL to transform the SDK and sample to  Keil project,but the MCUXPRESSO CONFIG give a error:

the mean is:the device detected from the project is not the same to the given device (MK20DX256xxx10), so the generated keil project ,i can open and build with no any error,but all the information about the device is KN60DX10.

   I could not find a exactly sdk and develop board  according to MK20DX256VMD10(MK20DXXX),What can i do ?

          Thanks

0 项奖励
回复
1 回复

1,463 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @ww_dong ,

Yes, if you create a new project base on MK20DX256 SDK, the project is only for TWR-K60M100. All the SDKs are around TWR/FRDM board.

You can replace those K60 files with K20 files manually.  But that's a bit boring. 

 

Regards,

Jing

0 项奖励
回复