SD card 4 bit mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD card 4 bit mode

1,964 Views
chobin
Contributor III

Hi everyone,

I'm developing a project where i'm using kinetis K20 microcontroller where I need to improve the SD card speed communication. Now it's working in 1 bit mode.

Did someone use SD card in 4 bit mode? I tried to develop the SDHC.c file using processor expert 10.2 where I selected 4 bit mode, but the SD card speed doesn't increase.

Does someone help me to start this 4 bit mode?

If I want to switch from SDHC mode to SPI mode, how I can do it?

Many thanks for your support.

Best regards,

Stefano

0 Kudos
Reply
1 Reply

1,438 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Chobin,

I'd like to share a project about Fat File System for SD card using SPI for K20.

The link as below.

Sd-Card Fat file system Project for Freescale Kinetis.rar
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply