Hi XiangJun Rong,
Thanks a lot for the response,
We are using the LDO to give constant supply to the MCU.
Battery Supply is connected to LDO and LDO ouput is connected to MCU-VDD pin.
LDO Part number - BD450M2EFJ-CE2
Atttached the LDO Circuit , MCU Connection in schematic and Data sheet of LDO.
Summarizing the Quries:
1. Any Idea Why MCU is not comes to normal mode, if we increase the voltage slow sequence(step by step).?
2.Attached waveform is right sequence for the MCU during supply voltage variation from 2 to 12 V?
3.Can you please provide how the MCU-PMU will behave during the sequence mentioned in the first comment.?
4. Is there specific configuration we have to do in MCU-PMU module ?
Thanks,
Muthu