Hello,
i'm trying do write some data into the EEPROM of the S9KEAZN32M4 with Segger Jlink. I can connect, flash a hex-File and read out register. For example the UUID with
mem8 40048010 8
i get 40048010 = 31 45 33 37 18 68 14 1E
So the connection should be ok.
I have to write 0x0B to 1000_0020 into the EEPROM. But when i write with
w1 10000020 0B
and read out with
mem8 10000020 8
i get
10000020 = FF FF FF FF FF FF FF FF.
Register 4002_0009 is set to 0x87, so EEPROM protection should be off.
Does anyone have an idea what's wrong on my side?
best regards