S32K148 FlexRAM non-writable size is 512 bytes after flash erase

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 FlexRAM non-writable size is 512 bytes after flash erase

Jump to solution
1,906 Views
warai
Contributor II

Hi All,

I did the following and the checked that the S32K148 FlexRAM non-writable size becomes 512 bytes. I know that if CSEC is enabled, I need to reserve 128 bytes but when I check the memory via the debugger I saw that I can't write to the last 512 bytes; i.e. Address 0x14000E00 - 0x14001000.

Did I break the flash?

0 Kudos
Reply
1 Solution
1,899 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

It can be 512 bytes depending on the partitioning.

danielmartynek_0-1614330024758.pngdanielmartynek_0-1614330024758.png

AN5401 Getting Started with CSEc Security Module:

danielmartynek_1-1614330089848.pngdanielmartynek_1-1614330089848.png

Regards,

Daniel

 

View solution in original post

0 Kudos
Reply
1 Reply
1,900 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

It can be 512 bytes depending on the partitioning.

danielmartynek_0-1614330024758.pngdanielmartynek_0-1614330024758.png

AN5401 Getting Started with CSEc Security Module:

danielmartynek_1-1614330089848.pngdanielmartynek_1-1614330089848.png

Regards,

Daniel

 

0 Kudos
Reply