S32K148 FlexRAM non-writable size is 512 bytes after flash erase

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 FlexRAM non-writable size is 512 bytes after flash erase

ソリューションへジャンプ
1,933件の閲覧回数
warai
Contributor II

Hi All,

I did the following and the checked that the S32K148 FlexRAM non-writable size becomes 512 bytes. I know that if CSEC is enabled, I need to reserve 128 bytes but when I check the memory via the debugger I saw that I can't write to the last 512 bytes; i.e. Address 0x14000E00 - 0x14001000.

Did I break the flash?

0 件の賞賛
返信
1 解決策
1,926件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

It can be 512 bytes depending on the partitioning.

danielmartynek_0-1614330024758.png

AN5401 Getting Started with CSEc Security Module:

danielmartynek_1-1614330089848.png

Regards,

Daniel

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,927件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

It can be 512 bytes depending on the partitioning.

danielmartynek_0-1614330024758.png

AN5401 Getting Started with CSEc Security Module:

danielmartynek_1-1614330089848.png

Regards,

Daniel

 

0 件の賞賛
返信