Routing through NC or unused MAPBGA pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Routing through NC or unused MAPBGA pins

3,298 次查看
malder
Contributor I

The 121 pin MAPBGA package (MK22FN256) has several 'NC' pins on the periphery of the package.

Routing would be made much easier if we could either route through these pads or not populate the pads at all.

Are either of these options possible?

0 项奖励
回复
4 回复数

3,154 次查看
bobpaddock
Senior Contributor IV

At my blog there are links to books on PCB layout including BGA routing: http://blog.softwaresafety.net/2010/03/survival-is-not-mandatory-right-first.html

0 项奖励
回复

3,154 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Matt

For NC pins. you can route through when you layout. For pins which have function but no used, you cannot route through.

Hope my reply can help you.

Best Regards

Paul

0 项奖励
回复

3,154 次查看
malder
Contributor I

Hi

Maybe I wasn't very clear...

I found this thread which suggests that 'NC' pins on the MK20 parts are used for internal testing, and so should not be connected to anything on the board.

NC pins on Kinetis K20 based MK20FN1M0VMD12 quick easy question

But the answer in that thread sounds very generic. So I am looking for confirmation.

I am using the MK22FN256 part and there are several NC pins on the periphery.

Are these pins connected internally?

If not, then I can route through them and it makes life much easier.

If they are used for testing etc then of course I will need to avoid them.

0 项奖励
回复

3,154 次查看
malder
Contributor I

Hi Paul,

That is very helpful.

However can I ask you to confirm that I can route through NC pads because I have since found this thread which seems to disagree:

NC pins on Kinetis K20 based MK20FN1M0VMD12 quick easy question

Thanks

Matt

0 项奖励
回复