Hi
Maybe I wasn't very clear...
I found this thread which suggests that 'NC' pins on the MK20 parts are used for internal testing, and so should not be connected to anything on the board.
NC pins on Kinetis K20 based MK20FN1M0VMD12 quick easy question
But the answer in that thread sounds very generic. So I am looking for confirmation.
I am using the MK22FN256 part and there are several NC pins on the periphery.
Are these pins connected internally?
If not, then I can route through them and it makes life much easier.
If they are used for testing etc then of course I will need to avoid them.