Required Part number for digital signage project.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Required Part number for digital signage project.

908 次查看
punithb
Contributor I

Hi All,

For our product design ,  we need low power micro controller which should able to drive 800*480 TFT  LCD display and also it should have bluetooth low energy capabilities so it can communicate to smart phone. Kindly suggest good  micro controller for this.


If any alternative like by adding additional hardware is also ok, suggest us.

Regards

Punith

0 项奖励
回复
1 回复

785 次查看
david_diaz
NXP Employee
NXP Employee

Hello Punith,

I would like to recommend the Kinetis K70 120/150 MHz MCUs​.

The Kinetis K7x is a Low-power MCU with graphics LCD, connectivity and security.

Please find more information about this family at the following link:

http://www.freescale.com/files/32bit/doc/fact_sheet/KNTSK70FS.pdf

Using the UART or SPI module from the device mentioned, it can communicate with an external Bluetooth device chip.

Hope this information will be useful for you.

Have a great day :smileyhappy:

David Diaz

0 项奖励
回复