Regarding the measurement of the PWM output and duty cycle as well as frequency input of the FTM of

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding the measurement of the PWM output and duty cycle as well as frequency input of the FTM of

2,051 Views
abyssnone
Contributor II

Hello!

I control one FTM to output PWM, and another FTM to measure the output PWM. When the frequency exceeds 10 kHz, the deviation between the measured frequency and duty cycle value and the actual value will increase as the input frequency increases. Moreover, why the PWM I output cannot be less than 25 Hz? Below 25 Hz, there is no output.

Please help me answer this question. Thank you very much!

0 Kudos
Reply
4 Replies

1,896 Views
abyssnone
Contributor II
Sorry, I'm not able to provide the entire code. I can only offer the relevant parts mentioned above.
0 Kudos
Reply

1,860 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @abyssnone ,

Could you tell me which MCU you are using? Specifically, I’m referring to its part number. Additionally, are you using a custom board or our FRDM board?
Which demo based on which SDK version are you using for testing?

BRs

Celeste

0 Kudos
Reply

1,840 Views
abyssnone
Contributor II
References the input_capture, dual_edge_capture, and simple_PWM engineering files. The chip is MKE13z.
0 Kudos
Reply

2,012 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Abyssnone,

Would you please confirm which MCU you are using and if it's an NXP board or a Custom board? If you would please also include IDE and SDK version it would help us.

Regards,
Gustavo

0 Kudos
Reply