Regarding USB multilink Universal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding USB multilink Universal

2,220件の閲覧回数
sheillysharma
Contributor I

Hello,

I am using USB MULTILINK UNIVERSAL tool  and facing problem in programming our kintex k61 micro-controller with part number MK61FX512VMJ12.

When we are trying to program,it's asking for firmware update and i have updated firmware 6.10 and code warrior which i am using is 10.5.
whether i need to update code warrior too.The snap shot of error is attached..
Thanks
Sheilly 
0 件の賞賛
返信
1 返信

2,160件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Please visit the P&E USB Multilink Universal Download link here to download [USB Multilink Universal (and FX) Resource CD], which Contains firmware update utility.

Please check if using that firm ware update utility could fix the issue.

If not, please update the CodeWarrior software to the latest Rev. 10.7

BTW: There is a note about CodeWarrior software doesn't support new Kinetis devices, more detailed info here.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信