Regarding Schematic SCH-27166REVC2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding Schematic SCH-27166REVC2

ソリューションへジャンプ
3,528件の閲覧回数
puspamnayak
Contributor III

Hi Community members,

I am using MK70FN1M0VMJ12 for the project and also using Tower EVM. In Tower EVM board we found reference of schematic SCH-27166REVC2.

Previously we were referring TWR-K70F120M-SCH which has Revision B1 and when I compared the TOWER EVM and schematic TWR-K70F120M-SCH REV B1, first difference i find is in connector J18 which is showing 3 Pin in  schematic TWR-K70F120M-SCH REV B1 whereas in Tower EVM board its 2 Pin Jumper.

So, I want to know what all are the changes done in TOWER EVM and also please send latest schematic SCH-27166REVC2 as referred by Tower EVM Board

Request you to reply at earliest

Regards,

Puspam Nayak

タグ(1)
0 件の賞賛
返信
1 解決策
3,361件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Puspam,

The Notes section of the RevC schematics indicae change do to FCC testing.

I have attached ZIP of the three schematic revisions I have.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,362件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Puspam,

The Notes section of the RevC schematics indicae change do to FCC testing.

I have attached ZIP of the three schematic revisions I have.

Regards,

David

0 件の賞賛
返信
3,361件の閲覧回数
puspamnayak
Contributor III

Hi David,

Thanks for your response but I am not able to find the attached ZIP file of the schematics you sent . Kindly resend the ZIP of the schematics again

Thanks and Regards,

Puspam N

0 件の賞賛
返信
3,361件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Puspam,

Are you looking at this in email or on the Freescale Community site?

The email will not have attachment.  The attachment can be received from the Community site:

Regarding Schematic SCH-27166REVC2 | Freescale Community

Regards,

David

0 件の賞賛
返信
3,361件の閲覧回数
puspamnayak
Contributor III

Hi David,

Thanks. I got the latest schematic and from Freescale Community site.

Please let me know if you have PCB Constraint document based on K70 design inetrfaced to DDR2, USB, NF, EEPROM, etc.

Kindly share the PCB constraint document which will help us in PCB design

Thanks and regards,

Puspam N

0 件の賞賛
返信