Reduce memory footprints in mbedtls

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reduce memory footprints in mbedtls

2,624件の閲覧回数
pritesh_shah
Contributor I

Hello,

I want to reduce the memory footprint of mbedtls library. I found the below link to optimize the mbedtls.

https://tls.mbed.org/kb/how-to/reduce-mbedtls-memory-and-storage-footprint

In this document one of the option is to save memory is to use mbedtls_x509_crt_parse_der_nocopy() function

instead of mbedtls_x509_crt_parse_der().

I have downloaded an SDK for Kinetis K64 and in that, i didn't found the mbedtls_x509_crt_parse_der_nocopy() function in mbedtls.

Is there any upgrade in the package ? How can i reduce the memory footprints for mbedtls. ?

タグ(2)
0 件の賞賛
返信
1 返信

2,540件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pritesh shah ,

  From the kinetis SDK x509_crt.c , this frile is part of mebd TSL(SSL Library mbed TLS / PolarSSL ).

  So, if you want to get the mbedtls_x509_crt_parse_der_nocopy() API, you may go the mbed side, find the newest driver which contains mbedtls_x509_crt_parse_der_nocopy() api function, and copy it to the SDK code.

  The newest SDK still didn't add the API which you mentione, but I think you can add it by yoursefl.

Wish it helps you!

Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信