Recommending Arduino shields that work with the FRDM board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recommending Arduino shields that work with the FRDM board

ソリューションへジャンプ
4,232件の閲覧回数
steve_fae
Senior Contributor I

What are the preferred shield boards that hopefully come with headers I can solder on and won't short out any power pins on the FRDM board?  I see a lot out there that say Arduino but they come in all shapes and sizes.   http://shieldlist.org/

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
3,725件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi Steven,

FRDM board is compatible with Arduino Uno R3

I hope this helps to select the shields eaiser.

Best Regards,

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,726件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi Steven,

FRDM board is compatible with Arduino Uno R3

I hope this helps to select the shields eaiser.

Best Regards,

Luis

0 件の賞賛
返信
3,724件の閲覧回数
steve_fae
Senior Contributor I

Thanks Luis, I think we will try to order some of these

http://www.arduinomall.com/artduino-proto-prototype-shield-diy-kit-for-a

rduino-uno-r3-mega-p-240.html

0 件の賞賛
返信