Recommended Bootloaders

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recommended Bootloaders

Jump to solution
2,316 Views
JustSomeGuy
Contributor II

I'm working with a K82 MCU and require a bootloader so that I can update my application over UART.  It looks like I shouldn't have to reinvent the wheel for this, but in my searching, I've come across several different bootloaders and it is not clear to me which are active and recommended.  Here are the bootloaders that I've found:

  1. Developer's Serial Bootloader (https://community.nxp.com/t5/Kinetis-Microcontrollers/Developer-s-Serial-Bootloader/ta-p/1104674)
  2. Kinetis Bootloader v2.0.0 (KBOOT aka MCUBOOT) (https://community.nxp.com/t5/MCU-Bootloader-Knowledge-Base/Introducing-Kinetis-Bootloader-v2/ta-p/11...)
  3. Freedom Bootloader (example project in MCUXpresso) - this looks related but substantially different than the Kinetis Bootloader v2.0.0
  4. uTaskerV1.4 (https://github.com/uTasker/uTasker-Kinetis)

Can anyone offer any guidance on which are recommended and under which use cases?  Documentation is spotty and dated and none of the options seem to acknowledge the existence of the others.

0 Kudos
Reply
1 Solution
2,286 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @JustSomeGuy ,

Thank you for your post. We recommend the third one, the Freedom Bootloader (example project in MCUXpresso). You can refer to Get Started with the MCU Bootloader for NXP microcontrollers | NXP Semiconductors for the operation steps.
Hope the above answer can help you. If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

Best Regards,

Celeste

View solution in original post

0 Kudos
Reply
1 Reply
2,286 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @JustSomeGuy ,

Thank you for your post. We recommend the third one, the Freedom Bootloader (example project in MCUXpresso). You can refer to Get Started with the MCU Bootloader for NXP microcontrollers | NXP Semiconductors for the operation steps.
Hope the above answer can help you. If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

Best Regards,

Celeste

0 Kudos
Reply