Hi notanivipul
Do you also set the ADC0->SC1[0] DIFF bit to 0?
Now, what's the issue you are meeting?
Do you try the SDK code, and modify the channel to ADC channel1:
SDK_2.6.7_FRDM-KW38\boards\frdmkw38\driver_examples\adc16\polling
The SDK can be downloaded from this link:
https://mcuxpresso.nxp.com/
Whether it works or not?
Please try the SDK ADC code at first.
Any updated information, just kindly let me know.
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------