Read from 0th index in SPI+DMA configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Read from 0th index in SPI+DMA configuration

974 Views
madhavaishriram
Contributor II
Hi All, We are using the MKE15Z256xxx7 controller for transfer and receive the data through SPI with DMA. The slave device we are using for SPI+DMA is PMOD-SF3 and trying to read and write data and it is working fine. Below is the read and write operations for slave device PMOD-SF3 WriteBuff[10u] = {0x02, 0x00, 0xff, 0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06}; ReadBuff[10u] = {0x03, 0x00, 0xff, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00}; First 4 bytes are command plus address in the read and write buffer. The write operation is fine and working using SPI+DMA, but after read operation ReadBuff is containing using it. ReadBuff = {0x00, 0x00, 0x00, 0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06} The first 4 bytes are empty or contains some garbase values. So the issue is to remove those first 4 bytes from the read buffer and data is read from 0th location of buffer using SPI+DMA. So is there any way to read it from 0th index after writing command + address or is there any another solution regarding this issue. - Is there anything like we can write the command and address first and we can read or write data. - Or is it possible to write the command and address from separate buffer and data from another buffer and both buffers will work at same time using DMA+SPI. - Is there any way to solve this issue using different method in SPI+DMA. Please if anyone is having any idea, please let us know how to read manipulate data in read buffer.
0 Kudos
Reply
1 Reply

942 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @madhavaishriram,

There is a similar question on this post: LPSPI + DMA Buffer start from 4th index - NXP Community, could you please check it?

Regards, Raul.