Re: Manufacturing programming of Kinets MK11DN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: Manufacturing programming of Kinets MK11DN

1,533 Views
miduo
NXP Employee
NXP Employee

Hi,

For manufacturing level programming of the Kinetis, we recommend the P&E Multilink Universal tool for example the Cyclone Max tool, which support standalone programming.

As for the software, we recommend the PROG software which comes with a command-line programmer (CPROG). CPROG can be used to automate and speed up the programming process by running a batch file.

P&E's technical support staff can help you in getting the PROG and CPROG software to work with your setup.

Best Regards,

Fang

1 Reply

1,386 Views
vladimirpavlovi
Contributor I

Thank you Fang ,

Does the PROG and CPROG support other devices as well?

In other words, could I make my own device based on FTDI chip and use PROG/CPROG?

regards.

Vladimir Pavlovic

0 Kudos
Reply