Re: Manufacturing programming of Kinets MK11DN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: Manufacturing programming of Kinets MK11DN

1,517件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

For manufacturing level programming of the Kinetis, we recommend the P&E Multilink Universal tool for example the Cyclone Max tool, which support standalone programming.

As for the software, we recommend the PROG software which comes with a command-line programmer (CPROG). CPROG can be used to automate and speed up the programming process by running a batch file.

P&E's technical support staff can help you in getting the PROG and CPROG software to work with your setup.

Best Regards,

Fang

1 返信

1,370件の閲覧回数
vladimirpavlovi
Contributor I

Thank you Fang ,

Does the PROG and CPROG support other devices as well?

In other words, could I make my own device based on FTDI chip and use PROG/CPROG?

regards.

Vladimir Pavlovic

0 件の賞賛
返信