RTC with VBAT - Bare Metal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC with VBAT - Bare Metal

2,383件の閲覧回数
weblar
Contributor V

I'm trying to get the RTC working on a Kinetis K60 which uses a coin cell for battery backup.

The problem I'm having is that when I reset the system, each time I attempt to read the RTC_TSR using the rtc_get_time function, I always get a TIF (time invalid) flag set in the status register. The only way this can work is if I write RTC_TSR = 0 in the initialization routine, which doesn't seem correct (its meant to be a battery backed-up register, no?).

I'm using the following code...

void rtc_init() {

  // Reset the RTC by setting and clearing the SWR bit in the control register

  RTC_CR |= RTC_CR_SWR_MASK;

  RTC_CR &= ~RTC_CR_SWR_MASK;

  RTC_TAR = 0xFFFFFFFF;

  // Enable the oscillator

  RTC_CR |= RTC_CR_OSCE_MASK;

  delay_ms(125);

  RTC_TCR = RTC_TCR_CIR(0) | RTC_TCR_TCR(0);

  //RTC_TSR = 0;

  RTC_TAR = 0;

  RTC_TPR = 0;

  // Enable the time counter

  RTC_SR |= RTC_SR_TCE_MASK;

}

void rtc_set_time(uint32_t ticks) {

  // Disable the RTC

  RTC_SR &= ~RTC_SR_TCE_MASK;

  // Set the new time since UNIX epoch (01/01/1970)

  RTC_TSR = ticks;

  // Enable the RTC

  RTC_SR |= RTC_SR_TCE_MASK;

}

void rtc_get_time(uint32_t *ticks) {

  uint32_t sr = RTC_SR;

  if (sr & RTC_SR_TIF_MASK) {

  // Time Invalid flag set

  }

  *ticks = RTC_TSR;

}

I'm well aware that I'm probably doing something stupid but I can't for the life of me figure it out.

Any suggestions are very welcome.

Thanks,

Kev

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,463件の閲覧回数
zhaohuiliu
NXP Employee
NXP Employee

Hi,

Please read TIF flag and TSR register description more carefully in RM. TSR must be initilized before you can use it. It is a design requirment.

0 件の賞賛
返信