RTC_LDD component

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC_LDD component

1,405 Views
YanBo
Contributor I

I want to generate a sequence of random number so i want to use the internal clock of this software, but i dont konw how to use the component RTC_LDD, anyone can help me? It seems like the input clock frequence can not be set to 1 sec but the notification said that it must be 1 sec. So i am a bit confused about that..

0 Kudos
Reply
1 Reply

1,391 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Which mcu and ide do you use?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply