RS485

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,826件の閲覧回数
moiz_husain
Contributor I

Hi I am using K20 controller , please can you provide a testing code for RS-485 or a demo project

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,281件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Freescale provides RS485 example code for K20 product based on MQX RTOS.

Please check the default path (C:\Freescale\Freescale_MQX_4_1\mqx\examples\rs485) to find that example.

Freescale MQX could be download here.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,282件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Freescale provides RS485 example code for K20 product based on MQX RTOS.

Please check the default path (C:\Freescale\Freescale_MQX_4_1\mqx\examples\rs485) to find that example.

Freescale MQX could be download here.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,281件の閲覧回数
moiz_husain
Contributor I

Hi,

Thanks I already done that

now please can you help me on SD card interface with SPI for K-20, because there is not any K-20 example for K-20

0 件の賞賛
返信
3,281件の閲覧回数
dave408
Senior Contributor II

moiz.husain, you are better off creating a new, separate question and then "mentioning" community members in your post with the @ notation.

0 件の賞賛
返信