ROM to RAM copy in the startup file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ROM to RAM copy in the startup file

Jump to solution
6,095 Views
durgasivakrishn
Contributor III

Hi,

I am using MK66FN2M0VLQ18 as I know in the startup file processor has to copy the contents of .data and .bss section from ROM(FLASH) to RAM but in the MK66 startup file nowhere they mentioned about it, can anyone give me clarity.

 

Thanks & Regards,

sivakrishna

Tags (2)
0 Kudos
Reply
1 Solution
6,075 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi durgasivakrishn,

   It's not the must item, if you are just a normal app, you can run it directly from the flash.

   You can use your startup file, but if you are using the flash bootloader, I suggest you copy to the internal RAM.

 

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

----------------------------------------------------------------------------- 

View solution in original post

0 Kudos
Reply
3 Replies
6,075 Views
durgasivakrishn
Contributor III

Hi,

Thanks for your response kerry,

I have a question is it necessary to move the content from ROM to RAM.

Here I am attaching the startup file from the NXP.

 

Thanks & Regards,

Sivakrishna

 

0 Kudos
Reply
6,076 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi durgasivakrishn,

   It's not the must item, if you are just a normal app, you can run it directly from the flash.

   You can use your startup file, but if you are using the flash bootloader, I suggest you copy to the internal RAM.

 

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

----------------------------------------------------------------------------- 

0 Kudos
Reply
6,078 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi durgasivakrishn,

   Please download the K66 SDK from this link:

   https://mcuxpresso.nxp.com/

    Generate the MCUXpresso IDE project, then import one SDK project, you can find in the startup_mk66f18.c have the code which you want.

  

__attribute__ ((section(".after_vectors.reset")))
void ResetISR(void) {

    // Disable interrupts
    __asm volatile ("cpsid i");


#if defined (__USE_CMSIS)
// If __USE_CMSIS defined, then call CMSIS SystemInit code
    SystemInit();

#else
    // Disable Watchdog
    //  Write 0xC520 to watchdog unlock register
    *((volatile unsigned short *)0x4005200E) = 0xC520;
    //  Followed by 0xD928 to complete the unlock
    *((volatile unsigned short *)0x4005200E) = 0xD928;
    // Now disable watchdog via STCTRLH register
    *((volatile unsigned short *)0x40052000) = 0x01D2u;
#endif // (__USE_CMSIS)

    //
    // Copy the data sections from flash to SRAM.
    //
    unsigned int LoadAddr, ExeAddr, SectionLen;
    unsigned int *SectionTableAddr;

    // Load base address of Global Section Table
    SectionTableAddr = &__data_section_table;

    // Copy the data sections from flash to SRAM.
    while (SectionTableAddr < &__data_section_table_end) {
        LoadAddr = *SectionTableAddr++;
        ExeAddr = *SectionTableAddr++;
        SectionLen = *SectionTableAddr++;
        data_init(LoadAddr, ExeAddr, SectionLen);
    }

    // At this point, SectionTableAddr = &__bss_section_table;
    // Zero fill the bss segment
    while (SectionTableAddr < &__bss_section_table_end) {
        ExeAddr = *SectionTableAddr++;
        SectionLen = *SectionTableAddr++;
        bss_init(ExeAddr, SectionLen);
    }

#if !defined (__USE_CMSIS)
// Assume that if __USE_CMSIS defined, then CMSIS SystemInit code
// will enable the FPU
#if defined (__VFP_FP__) && !defined (__SOFTFP__)
    //
    // Code to enable the Cortex-M4 FPU only included
    // if appropriate build options have been selected.
    // Code taken from Section 7.1, Cortex-M4 TRM (DDI0439C)
    //
    // Read CPACR (located at address 0xE000ED88)
    // Set bits 20-23 to enable CP10 and CP11 coprocessors
    // Write back the modified value to the CPACR
    asm volatile ("LDR.W R0, =0xE000ED88\n\t"
                  "LDR R1, [R0]\n\t"
                  "ORR R1, R1, #(0xF << 20)\n\t"
                  "STR R1, [R0]");
#endif // (__VFP_FP__) && !(__SOFTFP__)
#endif // (__USE_CMSIS)


#if !defined (__USE_CMSIS)
// Assume that if __USE_CMSIS defined, then CMSIS SystemInit code
// will setup the VTOR register

    // Check to see if we are running the code from a non-zero
    // address (eg RAM, external flash), in which case we need
    // to modify the VTOR register to tell the CPU that the
    // vector table is located at a non-0x0 address.
    unsigned int * pSCB_VTOR = (unsigned int *) 0xE000ED08;
    if ((unsigned int *)g_pfnVectors!=(unsigned int *) 0x00000000) {
        *pSCB_VTOR = (unsigned int)g_pfnVectors;
    }
#endif // (__USE_CMSIS)
#if defined (__cplusplus)
    //
    // Call C++ library initialisation
    //
    __libc_init_array();
#endif

    // Reenable interrupts
    __asm volatile ("cpsie i");

#if defined (__REDLIB__)
    // Call the Redlib library, which in turn calls main()
    __main();
#else
    main();
#endif

    //
    // main() shouldn't return, but if it does, we'll just enter an infinite loop
    //
    while (1) {
        ;
    }
}


__attribute__ ((section(".after_vectors.init_data")))
void data_init(unsigned int romstart, unsigned int start, unsigned int len) {
    unsigned int *pulDest = (unsigned int*) start;
    unsigned int *pulsrc=(unsigned int*) romstart;
    unsigned int loop;
    for (loop = 0; loop < len; loop = loop + 4)
        *pulDest++ = *pulSrc++;
}

__attribute__ ((section(".after_vectors.init_bss")))
void bss_init(unsigned int start, unsigned int len) {
    unsigned int *pulDest = (unsigned int*) start;
    unsigned int loop;
    for (loop = 0; loop < len; loop = loop + 4)
        *pulDest++ = 0;
}

 

In fact, you can consider, copy the flash data to the internal RAM directly.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

0 Kudos
Reply