R&D work to replace MK10DN32VFM5 with MK10DX32VFM5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

R&D work to replace MK10DN32VFM5 with MK10DX32VFM5

924件の閲覧回数
JRIIS
NXP Employee
NXP Employee

So I understand that N stand for No-Flex Flash Memory and X stands for Flex Flash Memory.

The X version has a dual Flash bank (2*32kB) and can be firmware updated in the field – swapping between the 2 banks.

Could you please confirm that the first 32KB memory will be the same – so it can be used as a replacement.

Some details:

MK10DN32VFM5: Kinetis K10: 50MHz Cortex-M4 Performance MCU, 32KB Flash, 8KB SRAM, 32-QFN

MK10DX32VFM5: Kinetis K10: 50MHz Cortex-M4 Performance MCU, 64KB Flash, 8KB SRAM, 32-QFN

If  MK10DX32VFM5 is not a drop in replacement with MK10DN32VFM5 then please describe the R&D effort it take to do the replacement?

This request is comming since the avalibility on MK10DX32VFM5 is better than MK10DN32VFM5.

Thanks,

/Jakob

ラベル(1)
0 件の賞賛
返信
1 返信

880件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Jakob,

There isn't any work need to be done to replace MK10DN32VFM5 with MK10DX32VFM5. They share same RM, DS and errata. They have same mask 4N86B.

Regards,

Jing

0 件の賞賛
返信