LPUAT config problem and old drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPUAT config problem and old drivers

8,206 Views
va_ita
Contributor I

Buongiorno,

vi vorrei proporre alla vostra attenzione questo problema al quale non riesco a trovare soluzione.

in allegato vi allego una foto della scermata.

Non riesco ad allineare le versioni del driver LPUART e usando una versione più recente nel compilare il progetto mi restituisce gli errori in foto.

chiedo gentilmente un aiuto per risolvere il problema.

grazie anticipatamente

Vanny Cecchinato

Tags (1)
0 Kudos
Reply
3 Replies

8,135 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Vanny Cecchinato,

 Please write your question in English again, because I can't read your language.

  In fact, you can use the SDK code for your chip directly, it has the UART project.

  You can download the kinetis SDK code from this link:

Welcome | MCUXpresso SDK Builder 

  From your picture, seems you already use the SDK code.

  Do you meet the build issues with the KW36 SDK code? Which version? I find the newest version is:SDK_2.2.4_FRDM-KW36

  Your picture issue is using the item which the structure don't have.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

8,135 Views
va_ita
Contributor I

Hi Kerry Zhou, 

Sorry about Italian language. 

I found and install the new SDK 2.2.4 of MKW36Z512VHT4 (without board selection) but the driver of LPUART and GPIO isn't again aligned.

If necessary I sent you another photo of the problem that I have. 

Thank you so much

0 Kudos
Reply

8,135 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Vanny Cecchinato,

   Thanks for your updated information.

   Could you please create your KW36 issues in the following post again:

Wireless Connectivity 

   The KW series normally supported in the wireless forum, our related KW engineer will help you.

   This kinetis forum is mainly for the general MCU, not the KW series.

  Thanks a lot for your understanding.

Best Regards,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply