Question regarding clearing K64 FTM channel interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question regarding clearing K64 FTM channel interrupt

跳至解决方案
1,734 次查看
matthewwatson
Contributor I

The K64 reference manual describes the CHF channel interrupt flag in CnSC as:

Set by hardware when an event occurs on the channel. CHF is cleared by reading the CSC register while CHnF is set and then writing a 0 to the CHF bit. Writing a 1 to CHF has no effect. If another event occurs between the read and write operations, the write operation has no effect; therefore, CHF remains set indicating an event has occurred. In this case a CHF interrupt request is not lost due to the clearing sequence for a previous CHF.

This implies that no interrupts will be dropped that occur between reading the interrupt flag and resetting it by writing a 1.

However, the processor expert component interacts with this register three times. It is first read to check the status of the flag, the ISR is called, then the &= operation is used to reset the flag, effectively a read operation immediately followed by a write.

My question is does the description in the datasheet guarantee no loss of interrupt events between the first read operation and the write, or only between the second read and the write?

标记 (2)
0 项奖励
回复
1 解答
1,550 次查看
mjbcswitzerland
Specialist V

Matthew

I can confirm that the PE generated code will cause any interrupt event to be lost that occurs between the entry into the interrupt handler and resetting the flag.

1.
IRQ()

{

FTM0_SC &= ~(FTM_SC_TOF);

do stuff...

}

any further interrupt event that arrives after FTM0_SC is read will be pending at the end of the handler and cause it to be re-entered again.

2.

IRQ()

{

(void)FTM0_SC;

do stuff...

FTM0_SC &= ~(FTM_SC_TOF);

}

any further interrupt event that arrives after FTM0_SC is read will reset by the FTM0_SC &= ~(FTM_SC_TOF); and thus lost

3.

IRQ()

{

unsigned long temp = FTM0_SC;

do stuff...

FTM0_SC = (temp & ~(FTM_SC_TOF));

}

any further interrupt event that arrives after FTM0_SC is read on entry will be pending at the end of the handler (will not be reset by the clear of FTM_SC_TOF) and cause it to be re-entered again.

There are some instances where method 2 has an advantage because interrupt arriving faster than the handling rate will not cause the interrupt to always remain pending. In 99.999% of real use 2. is however incorrect code.

PE code may appear to work correctly but it makes sense to always check carefully because it may not satisfy real developments requirements without some "tuning".

Regards

Mark

在原帖中查看解决方案

3 回复数
1,550 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Matthew Watson,

In the &= operation, a read operation immediately followed by a write is executed.

The process of the operation shouldn't be interfered.

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,551 次查看
mjbcswitzerland
Specialist V

Matthew

I can confirm that the PE generated code will cause any interrupt event to be lost that occurs between the entry into the interrupt handler and resetting the flag.

1.
IRQ()

{

FTM0_SC &= ~(FTM_SC_TOF);

do stuff...

}

any further interrupt event that arrives after FTM0_SC is read will be pending at the end of the handler and cause it to be re-entered again.

2.

IRQ()

{

(void)FTM0_SC;

do stuff...

FTM0_SC &= ~(FTM_SC_TOF);

}

any further interrupt event that arrives after FTM0_SC is read will reset by the FTM0_SC &= ~(FTM_SC_TOF); and thus lost

3.

IRQ()

{

unsigned long temp = FTM0_SC;

do stuff...

FTM0_SC = (temp & ~(FTM_SC_TOF));

}

any further interrupt event that arrives after FTM0_SC is read on entry will be pending at the end of the handler (will not be reset by the clear of FTM_SC_TOF) and cause it to be re-entered again.

There are some instances where method 2 has an advantage because interrupt arriving faster than the handling rate will not cause the interrupt to always remain pending. In 99.999% of real use 2. is however incorrect code.

PE code may appear to work correctly but it makes sense to always check carefully because it may not satisfy real developments requirements without some "tuning".

Regards

Mark

1,550 次查看
matthewwatson
Contributor I

This is exactly what I suspected, thanks for the clarification Mark!

0 项奖励
回复