Question on KW45 Reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question on KW45 Reset

跳至解决方案
1,473 次查看
jictannu
Contributor III

Hi all,

I have a question regarding the reset process for KW45. Does the reset source mentioned in Chapter 22 of the KW45 Reference Manual cause both the cm33 and cm3 cores to reset simultaneously? Specifically, for a software reset, is it only requesting a reset for the cm33 core, without affecting the cm3 core?

Best regards,

jictannu

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,453 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @jictannu

Hope you are doing well.

Some reset requests can affect the CM3 for specific purposes such as debug or flash loading. Please, take a look at the KW45 Reference Manual, Chapter 53 Radio Platform, Section 53.3.5.6 RFMC > Reset; and Chapter 55 RF Core Mode Controller.

Regards,
Eduardo.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,454 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @jictannu

Hope you are doing well.

Some reset requests can affect the CM3 for specific purposes such as debug or flash loading. Please, take a look at the KW45 Reference Manual, Chapter 53 Radio Platform, Section 53.3.5.6 RFMC > Reset; and Chapter 55 RF Core Mode Controller.

Regards,
Eduardo.

0 项奖励
回复