Question on KW45 Reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question on KW45 Reset

ソリューションへジャンプ
2,138件の閲覧回数
jictannu
Contributor III

Hi all,

I have a question regarding the reset process for KW45. Does the reset source mentioned in Chapter 22 of the KW45 Reference Manual cause both the cm33 and cm3 cores to reset simultaneously? Specifically, for a software reset, is it only requesting a reset for the cm33 core, without affecting the cm3 core?

Best regards,

jictannu

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,118件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @jictannu

Hope you are doing well.

Some reset requests can affect the CM3 for specific purposes such as debug or flash loading. Please, take a look at the KW45 Reference Manual, Chapter 53 Radio Platform, Section 53.3.5.6 RFMC > Reset; and Chapter 55 RF Core Mode Controller.

Regards,
Eduardo.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,119件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @jictannu

Hope you are doing well.

Some reset requests can affect the CM3 for specific purposes such as debug or flash loading. Please, take a look at the KW45 Reference Manual, Chapter 53 Radio Platform, Section 53.3.5.6 RFMC > Reset; and Chapter 55 RF Core Mode Controller.

Regards,
Eduardo.

0 件の賞賛
返信