Question about switching to VLPR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about switching to VLPR

1,378件の閲覧回数
vt100
Contributor I

According to the K70 User Manual, when switching to VLPR there is a delay between setting the RUNM field in SMC_PMCTRL and completing the transition to VLPR.
How will the K70 behave if an attempt to switch to WAIT mode occurs during this delay?
Will the K70 switch to WAIT mode, VLPW mode, or is the behavior undefined?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,242件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi

Thank you very much for your focus on Freescale Kinetis product.

The datasheet also hasn't illustrated the result happen when execute the enter WAIT mode during entering the VLPR mode.

And I'd highly recommend that avoid the this execution.

Hope it helps,
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信