Question about pin headers on Kinetis KL25Z based Freedom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about pin headers on Kinetis KL25Z based Freedom board

ソリューションへジャンプ
2,332件の閲覧回数
williamstapleto
Contributor I

I recently received the KL25Z based Freedom board and was trying to match the pin configurations on the board to the pins coming from the chip in order to map the placement of resources.

On the back of the freedom board, there is a silk-screened pin map which includes the following pins listed: C20, C21, C22, C23, C29, and C30.

As far as I can tell from the KL25Z datasheet, no such pins exist.

However, pins E20, E21, E22, E23, E29, and E30 exist.

Could I get official confirmation that these pins on the Freedom board header are the port E pins?

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,956件の閲覧回数
Smiffytech
Contributor III

I think your best reference is the actual schematics:

http://cache.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL25Z_SCH.pdf?fsrch=1...

I found that silkscreen just plain confusing. Reading the top of the board, you can see J2, J1, J9, J10 - which all match up with the schematic, which is marked with the actual MCU pin designations.

Hope this helps!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,957件の閲覧回数
Smiffytech
Contributor III

I think your best reference is the actual schematics:

http://cache.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL25Z_SCH.pdf?fsrch=1...

I found that silkscreen just plain confusing. Reading the top of the board, you can see J2, J1, J9, J10 - which all match up with the schematic, which is marked with the actual MCU pin designations.

Hope this helps!

0 件の賞賛
返信