Question About SPI Module "DSPI" MCR register Configuration.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question About SPI Module "DSPI" MCR register Configuration.

ソリューションへジャンプ
2,345件の閲覧回数
islamwahdan
Contributor I

For the SPI module  DSPI_x the MCR register contains bit fields [PCSIS0....PCSISn] ...i am operating the MCU in slave mode is PCSIS0 now my chip select (CS0).......[i.e PCSIS1 = CS1 , PCSIS2 = CS2 and so on....]?]

タグ(2)
0 件の賞賛
返信
1 解決策
2,134件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Islam,

You're 100% correct. Only the PCS0/SS pin support the slave operation and other PCS pins become invalid when work in slave mode.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,134件の閲覧回数
pietrodicastri
Senior Contributor II

Hello

I am now wondering the same thing. Did You figure out??

I wander what is the sense of having more than one SS for one slave instance..

Thank You

Pietro

0 件の賞賛
返信
2,134件の閲覧回数
islamwahdan
Contributor I

Hello Pietro

I think yes PCSIS0 (CS0) is the only active chip select in slave mode , the other CS i think are for Master Mode only, i didn't get any confirmation from anyone though.

thanks

0 件の賞賛
返信
2,135件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Islam,

You're 100% correct. Only the PCS0/SS pin support the slave operation and other PCS pins become invalid when work in slave mode.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信