QEI inputs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,890件の閲覧回数
marcelo_freek
Contributor I

I´m looking for a Kinetis with quadrature encoder input.

 

None found. Is it correct  ?

 

Thanks.

0 件の賞賛
返信
1 解決策
3,457件の閲覧回数
apanecatl
Senior Contributor II

All the kinetis microcontrollers feature one or more FlexTimers (FTM) which supports Quadrature decoder with input filters, relative position counting, and interrupt on position count or capture of position count on external event

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,457件の閲覧回数
JimDon
Senior Contributor III

Just one problem with that answer - it is not correct. Not all Kinetis MCUs have a an FTM.

It seems you are not the only one with this mistaken notion. On the Freedom Board they pinned it out as FTM, when in fact it is TPM.

Example:

The KL25 Has a TPM, quoting from the RM:

(Document Number: KL25P80M48SF0RM)

"The TPM is built upon a very simple timer (HCS08 Timer PWM Module – TPM) used

for many years on Freescale's 8-bit microcontrollers. The TPM extends the functionality

to support operation in low power modes by clocking the counter, compare and capture

registers from an asynchronous clock that can remain functional in low power modes"

0 件の賞賛
返信
3,457件の閲覧回数
apanecatl
Senior Contributor II

I forgot to mention I was referring to the K family

0 件の賞賛
返信
3,458件の閲覧回数
apanecatl
Senior Contributor II

All the kinetis microcontrollers feature one or more FlexTimers (FTM) which supports Quadrature decoder with input filters, relative position counting, and interrupt on position count or capture of position count on external event

0 件の賞賛
返信
3,457件の閲覧回数
mf_kappa
Contributor II

Hi

See K-40 Series, With Flex timer peripheral.

Has option to Quadrature Decoder mode

0 件の賞賛
返信