QEI inputs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QEI inputs

Jump to solution
3,925 Views
marcelo_freek
Contributor I

I´m looking for a Kinetis with quadrature encoder input.

 

None found. Is it correct  ?

 

Thanks.

0 Kudos
Reply
1 Solution
3,492 Views
apanecatl
Senior Contributor II

All the kinetis microcontrollers feature one or more FlexTimers (FTM) which supports Quadrature decoder with input filters, relative position counting, and interrupt on position count or capture of position count on external event

View solution in original post

0 Kudos
Reply
4 Replies
3,492 Views
JimDon
Senior Contributor III

Just one problem with that answer - it is not correct. Not all Kinetis MCUs have a an FTM.

It seems you are not the only one with this mistaken notion. On the Freedom Board they pinned it out as FTM, when in fact it is TPM.

Example:

The KL25 Has a TPM, quoting from the RM:

(Document Number: KL25P80M48SF0RM)

"The TPM is built upon a very simple timer (HCS08 Timer PWM Module – TPM) used

for many years on Freescale's 8-bit microcontrollers. The TPM extends the functionality

to support operation in low power modes by clocking the counter, compare and capture

registers from an asynchronous clock that can remain functional in low power modes"

0 Kudos
Reply
3,492 Views
apanecatl
Senior Contributor II

I forgot to mention I was referring to the K family

0 Kudos
Reply
3,493 Views
apanecatl
Senior Contributor II

All the kinetis microcontrollers feature one or more FlexTimers (FTM) which supports Quadrature decoder with input filters, relative position counting, and interrupt on position count or capture of position count on external event

0 Kudos
Reply
3,492 Views
mf_kappa
Contributor II

Hi

See K-40 Series, With Flex timer peripheral.

Has option to Quadrature Decoder mode

0 Kudos
Reply