Protoboard advice for FRDM-K64F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Protoboard advice for FRDM-K64F

ソリューションへジャンプ
2,403件の閲覧回数
olivierkieffer
Contributor II


I'm looking for a protoboard for FRDM-K64F. I know this board is compatible with Arduino headers, but I want to use CAN controller feature directly from K64 (not through SPI -Arduino- shield). As far as I understand the pinout, CAN Rx/Tx are available on the Freescale I/O headers but not on the Arduino headers, so I can't use Arduino protoboard.

I would need a prototoboard (to add a CAN transceiver and some other components)  with all Arduino and Freescale I/O headers available.

Any advice?

Thanks

ラベル(2)
0 件の賞賛
返信
1 解決策
2,161件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Olivier,

Unfortunately, NXP hasn't provided some kinds of the protoboard just as you want, and I'd like to suggest that you can give a try on eBay.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,162件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Olivier,

Unfortunately, NXP hasn't provided some kinds of the protoboard just as you want, and I'd like to suggest that you can give a try on eBay.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,161件の閲覧回数
olivierkieffer
Contributor II

Hi Jeremy,

I did not find any 3rd party neither. I will just make my own board.

Thanks for your help.

Olivier

0 件の賞賛
返信