Programming Manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,133件の閲覧回数
markusbraitner
Contributor IV

Hi,

I'm currently evaluating K60 using a TWR-K60D100M Tower System. Is there a programming manual (showing which ASM commands are available etc.) available from Freescale for this kind of processor? So far I've only found Data Sheets and Reference Manuals on the Freescale website...

Kind regards,

Markus

ラベル(1)
タグ(4)
1 解決策
3,676件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Markus,

The Kinetis K60 has an ARM Cortex M4 Core, all the documentation related to the core is provided by ARM. Kinetis Reference Manuals and Datasheets provided by Freescale contain information about the peripheral modules.

In the links below you can find information that may help.

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0553a/CIHJJEIH.html

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0439b/CHDDIGAC.html

http://infocenter.arm.com/help/topic/com.arm.doc.ddi0439d/DDI0439D_cortex_m4_processor_r0p1_trm.pdf

Best regards,

Carlos

元の投稿で解決策を見る

3 返答(返信)
3,677件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Markus,

The Kinetis K60 has an ARM Cortex M4 Core, all the documentation related to the core is provided by ARM. Kinetis Reference Manuals and Datasheets provided by Freescale contain information about the peripheral modules.

In the links below you can find information that may help.

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0553a/CIHJJEIH.html

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0439b/CHDDIGAC.html

http://infocenter.arm.com/help/topic/com.arm.doc.ddi0439d/DDI0439D_cortex_m4_processor_r0p1_trm.pdf

Best regards,

Carlos

3,677件の閲覧回数
frank涛李
Contributor II

Hi Carlos,

Thanks a lot.It does help me!

Best regards,

Frank

0 件の賞賛
返信
3,676件の閲覧回数
markusbraitner
Contributor IV

Hi Carlos,

thank you for your fast and helpful response!

Greetings,

Markus

0 件の賞賛
返信